This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3104: Discrepancy in datasheet? Please clarify.

Part Number: TLV320AIC3104

Hello. I'm trying to get some analog sound out of a TLV320AIC3104 codec. I downloaded the latest revision (revision F) of the datasheet here.

I believe there is an error on page 18, on the functional block diagram. See the highlighted path for DAC_R1 to LEFT_LOP/M.

This path suggests that the DAC_R1 signal is connected directly to the LEFT_LOP/M driver. Not passing through the mixer.

On page 33 there is another diagram that details the output stage for line output drivers:

This one suggests that the signal DSC_R1 is connected to the input of the ouput stage mixers, which contradicts the previous diagram.

Which one is correct?

I'm thinking that if I want both DAC's outputs on headphones and line outputs, I need to route the output of the ADCs to DAC_R1 and DACL1 and set the mixer levels. Is this correct?

Thanks in advance.