Hi,
I'm evaluating the PCM9211EVM-U by using the CodecControl on Window 10, the CodecControl shows that the USB Fs = 44100, then I use the Saleae Logic to capture the I2S signal on the bus, shows that the I2S WCLK is running at 48 kHz, which is not match the 44.1k Hz. Then I also change the tas1020b firmware to someother frequency value, i.e. USB-miniEVM0204 with 16 kHz, 24 kHz, 32 kHz, etc, however, the I2S WCLK at the PCM9211EVM-U always running at 48 kHz, not matter how I set the tas1020b firmware with different frequency, or change the default format in the window control panel sound configuration.
Is it a way to fix the I2S WCLK on the PCM9211EVM-U to a correct frequency?