Hello,
I have questions about both TAS5411-Q1 data sheet and EVM.
-DataSheet (Page.4)
7.1 Absolute Maximum Ratings
The max value of the input voltage for SCL, SDA, STANDBY pins are 5 V,
but the values of V (IH_SCL) , V (IH_SDA) listed on the next page are MAX 5.5 V.
Are the Absolute Maximum Ratings of SCL, SDA, / STANDBY pins the same value as For IN IN, IN _ P, and MUTE pins,MAX 6.5 V?
-TAS5411EVM User's Guide (Page.9-10)
Is L1 (Inductor) placed on the power line (VIN) of TAS5411 EVM a filter for power supply?
Thank you for your help.
Best Regards, Orobianco