Hello,
I have a custom board, with tlv320aic3100 codec connected to it.
I would like to ask a question regarding the headset detection using tlv320aic3100 codec:
From s/w i have enabled the d7 bit in the page 0 register 67, and also the debounce time to 256 msec => 0x90
Then, in the page 0 reg 48 i have enabled the headset insertion detect interrupt generation d7 bit.
but in the the detection is not happening as: in the page 0 register 46 the bit d4 is always set to 1 no matter headset is connected or removed. This i tried with more than 10 different headsets.
TI can you please help ?
thanks,
aniket