This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM49352 do not work

Hello,

We're using LM49352 as an audio codec. The project basic information list as bellows,

Linux Kernel -- 3.14.52

Audio formats -- PCM (slave)

NO MCLK,  use PORT1_CLK  (2.048MHz)

sampling frequency -- 8kHz

Registers config :

{ 0x00, 0x29 }, { 0x01, 0x01 }, { 0x10, 0x03 }, { 0x20, 0x12 },
{ 0x30, 0x11 }, { 0x44, 0x09 }, { 0x50, 0x21 }, { 0x54, 0x1b },
{ 0x55, 0x02 }, { 0x56, 0x02 },

But, the codec is not working. 

Can any one help me here, thanks in advance!