Part Number: TLV320AIC3254
Hi team,
My customer is using AIC3254 in an infotainment project, the tuner is input from IN2_R/L, and the USB is input from I2S.
And customer found that, when the whole system power on, if I turn on tuner firstly, there is no sound. I have to turn on USB firstly and then turn it off, and then turn on tuner, only with this sequence the tuner will work well.
And we have tried to set the I2S clock as master mode during tuner is on, but nothing change.
So I wondering if you have met similar issue and any solution towards it?
W30 00 00
W30 1B 0C
W30 1E 84
Thank you.