This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRC4190: SRC4190 input sampling rate range

Part Number: SRC4190

Hi,

We are looking for suitable SRC chip which can handle a wide range of input sampling rate and the output sampling rate will be fixed at 48kHz or 96kHz. It seems that SRC4190 is a right choice, I would like to confirm that it can support the following input sampling rate or not if I fixed the RCKI at 12.288Mhz.

Input sampling rate = 8, 11.025, 12, 16, 22.05, 32, 44.1, 48, 64, 88.2, 96 kHz

Regards,

Stephen