This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Starterware/TLV320DAC3100: TLV320DAC3100 speaker sound small after the boot

Part Number: TLV320DAC3100

Tool/software: Starterware

The machine has Speaker and Line out, all through the 3100 output, the master through the I2S, I2C send data and configuration 3100.

After the boot, Speaker sound is very small (regardless of volume, even if the volume is transferred to the maximum, the sound is very small and no change), and Line Out is able to normal output, adjust the volume will respond.

3100 all the power supply are normal supply, through the oscilloscope monitoring, there has been no power-down phenomenon, only to restart the machine to return to normal.

I2C rate of 100K, and the master will be in the boot process before and after 2 times through the I2C configuration 3100.

Reproduction probability: 30%, attachment for register configuration.

Above, please help analyze the reasons, thank you!

<4>[   26.291855] addr 0x00: write:0x00 ,read:0x00
<4>[   26.292973] addr 0x01: write:0x01 ,read:0x00
<4>[   26.294078] addr 0x04: write:0x07 ,read:0x07
<4>[   26.295192] addr 0x06: write:0x07 ,read:0x07
<4>[   26.296389] addr 0x07: write:0x00 ,read:0x00
<4>[   26.297054] addr 0x08: write:0x00 ,read:0x00
<4>[   26.298137] addr 0x05: write:0x94 ,read:0x94
<4>[   26.299296] addr 0x0b: write:0x82 ,read:0x82
<4>[   26.300440] addr 0x0c: write:0x87 ,read:0x87
<4>[   26.301620] addr 0x0d: write:0x00 ,read:0x00
<4>[   26.302285] addr 0x0e: write:0x80 ,read:0x80
<4>[   26.303406] addr 0x1b: write:0x00 ,read:0x00
<4>[   26.304520] addr 0x3c: write:0x02 ,read:0x02
<4>[   26.305640] addr 0x00: write:0x00 ,read:0x00
<4>[   26.306793] addr 0x74: write:0x00 ,read:0x00
<4>[   26.307920] addr 0x00: write:0x01 ,read:0x01
<4>[   26.309037] addr 0x1f: write:0x14 ,read:0x14
<4>[   26.310178] addr 0x21: write:0x4e ,read:0x4e
<4>[   26.311299] addr 0x23: write:0x44 ,read:0x44
<4>[   26.312516] addr 0x28: write:0x0e ,read:0x0e
<4>[   26.313206] addr 0x29: write:0x0e ,read:0x0e
<4>[   26.314316] addr 0x2a: write:0x0c ,read:0x0c
<4>[   26.315455] addr 0x1f: write:0xd6 ,read:0xd6
<4>[   26.316840] addr 0x20: write:0x86 ,read:0x86
<4>[   26.317949] addr 0x24: write:0x80 ,read:0x80
<4>[   26.319053] addr 0x25: write:0x80 ,read:0x80
<4>[   26.320192] addr 0x26: write:0x8e ,read:0x8e
<4>[   26.320205] sleep 50ms
<4>[   26.361222] addr 0x00: write:0x00 ,read:0x00
<4>[   26.362364] addr 0x3f: write:0xfc ,read:0xfc
<4>[   26.363595] addr 0x41: write:0x0a ,read:0x0a
<4>[   26.364379] addr 0x42: write:0x0a ,read:0x0a
<4>[   26.366059] addr 0x40: write:0x0e ,read:0x0e

<4>[   26.367206] addr 0x00: write:0x01 ,read:0x01
<4>[   26.370554] addr 0x23: write:0x44 ,read:0x44
<4>[   26.371978] addr 0x00: write:0x00 ,read:0x00
<4>[   26.373168] addr 0x40: write:0x0e ,read:0x0e
<4>[   26.374311] addr 0x00: write:0x01 ,read:0x01
<4>[   26.375540] addr 0x28: write:0x02 ,read:0x02
<4>[   26.376405] addr 0x29: write:0x02 ,read:0x02
<4>[   26.377581] addr 0x2a: write:0x08 ,read:0x08
<4>[   26.378746] addr 0x20: write:0x06 ,read:0x06
<4>[   26.379874] addr 0x00: write:0x00 ,read:0x00
<4>[   26.381067] addr 0x44: write:0x61 ,read:0x61
<4>[   26.382361] addr 0x45: write:0x20 ,read:0x20
<4>[   26.384368] addr 0x46: write:0x6b ,read:0x6b
<4>[   26.385563] addr 0x00: write:0x08 ,read:0x08
<4>[   26.386725] addr 0x01: write:0x05 ,read:0x05
<4>[   26.388088] addr 0x01: write:0x05 ,read:0x05
<4>[   26.390239] addr 0x02: write:0x7f ,read:0x7f
<4>[   26.391027] addr 0x03: write:0x2d ,read:0x2d
<4>[   26.391790] addr 0x04: write:0x82 ,read:0x82
<4>[   26.392554] addr 0x05: write:0x39 ,read:0x39
<4>[   26.393296] addr 0x06: write:0x7c ,read:0x7c
<4>[   26.394034] addr 0x07: write:0x69 ,read:0x69
<4>[   26.394779] addr 0x08: write:0x7d ,read:0x7d
<4>[   26.395522] addr 0x09: write:0xc4 ,read:0xc4
<4>[   26.396282] addr 0x0a: write:0x84 ,read:0x84
<4>[   26.397029] addr 0x0b: write:0x63 ,read:0x63
<4>[   26.399226] addr 0x0c: write:0x6f ,read:0x6f
<4>[   26.399987] addr 0x0d: write:0xee ,read:0xee
<4>[   26.400841] addr 0x0e: write:0xa3 ,read:0xa3
<4>[   26.401618] addr 0x0f: write:0x70 ,read:0x70
<4>[   26.402345] addr 0x10: write:0x5e ,read:0x5e
<4>[   26.403084] addr 0x11: write:0x42 ,read:0x42
<4>[   26.403814] addr 0x12: write:0x5c ,read:0x5c
<4>[   26.404520] addr 0x13: write:0x90 ,read:0x90
<4>[   26.405220] addr 0x14: write:0xb1 ,read:0xb1
<4>[   26.405964] addr 0x15: write:0xce ,read:0xce
<4>[   26.407965] addr 0x16: write:0x77 ,read:0x77
<4>[   26.408678] addr 0x17: write:0x3f ,read:0x3f
<4>[   26.409379] addr 0x18: write:0xc1 ,read:0xc1
<4>[   26.410117] addr 0x19: write:0x54 ,read:0x54
<4>[   26.410832] addr 0x1a: write:0x59 ,read:0x59
<4>[   26.411538] addr 0x1b: write:0x53 ,read:0x53
<4>[   26.412259] addr 0x1c: write:0x3e ,read:0x3e
<4>[   26.412953] addr 0x1d: write:0xac ,read:0xac
<4>[   26.413654] addr 0x1e: write:0xaf ,read:0xaf
<4>[   26.414357] addr 0x1f: write:0x6d ,read:0x6d
<4>[   26.416429] addr 0x20: write:0x71 ,read:0x71
<4>[   26.417152] addr 0x21: write:0x05 ,read:0x05
<4>[   26.417846] addr 0x22: write:0x0f ,read:0x0f
<4>[   26.418540] addr 0x23: write:0xb1 ,read:0xb1
<4>[   26.419227] addr 0x24: write:0x3d ,read:0x3d
<4>[   26.419933] addr 0x25: write:0xce ,read:0xce
<4>[   26.420727] addr 0x26: write:0x00 ,read:0x00
<4>[   26.421469] addr 0x27: write:0x4f ,read:0x4f
<4>[   26.422212] addr 0x28: write:0xd1 ,read:0xd1
<4>[   26.422959] addr 0x29: write:0x2c ,read:0x2c
<4>[   26.425102] addr 0x2a: write:0x7f ,read:0x7f
<4>[   26.425874] addr 0x2b: write:0xb6 ,read:0xb6
<4>[   26.426726] addr 0x2c: write:0x80 ,read:0x80
<4>[   26.427741] addr 0x2d: write:0xae ,read:0xae
<4>[   26.428666] addr 0x2e: write:0x7e ,read:0x7e
<4>[   26.429444] addr 0x2f: write:0xfc ,read:0xfc
<4>[   26.430225] addr 0x30: write:0x7f ,read:0x7f
<4>[   26.430999] addr 0x31: write:0x52 ,read:0x52
<4>[   26.431813] addr 0x32: write:0x81 ,read:0x81
<4>[   26.432700] addr 0x33: write:0x4c ,read:0x4c
<4>[   26.433921] addr 0x01: write:0x05 ,read:0x05
<4>[   26.436966] addr 0x02: write:0x7f ,read:0x7f
<4>[   26.440220] addr 0x03: write:0x2d ,read:0x2d
<4>[   26.440985] addr 0x04: write:0x82 ,read:0x82
<4>[   26.441723] addr 0x05: write:0x39 ,read:0x39
<4>[   26.442464] addr 0x06: write:0x7c ,read:0x7c
<4>[   26.443203] addr 0x07: write:0x69 ,read:0x69
<4>[   26.443945] addr 0x08: write:0x7d ,read:0x7d
<4>[   26.444701] addr 0x09: write:0xc4 ,read:0xc4
<4>[   26.445433] addr 0x0a: write:0x84 ,read:0x84
<4>[   26.446168] addr 0x0b: write:0x63 ,read:0x63
<4>[   26.448202] addr 0x0c: write:0x6f ,read:0x6f
<4>[   26.448997] addr 0x0d: write:0xee ,read:0xee
<4>[   26.449766] addr 0x0e: write:0xa3 ,read:0xa3
<4>[   26.450503] addr 0x0f: write:0x70 ,read:0x70
<4>[   26.451233] addr 0x10: write:0x5e ,read:0x5e
<4>[   26.451957] addr 0x11: write:0x42 ,read:0x42
<4>[   26.452675] addr 0x12: write:0x5c ,read:0x5c
<4>[   26.453383] addr 0x13: write:0x90 ,read:0x90
<4>[   26.454096] addr 0x14: write:0xb1 ,read:0xb1
<4>[   26.454823] addr 0x15: write:0xce ,read:0xce
<4>[   26.457339] addr 0x16: write:0x77 ,read:0x77
<4>[   26.458090] addr 0x17: write:0x3f ,read:0x3f
<4>[   26.458862] addr 0x18: write:0xc1 ,read:0xc1
<4>[   26.459592] addr 0x19: write:0x54 ,read:0x54
<4>[   26.460455] addr 0x1a: write:0x59 ,read:0x59
<4>[   26.461239] addr 0x1b: write:0x53 ,read:0x53
<4>[   26.462039] addr 0x1c: write:0x3e ,read:0x3e
<4>[   26.462819] addr 0x1d: write:0xac ,read:0xac
<4>[   26.463563] addr 0x1e: write:0xaf ,read:0xaf
<4>[   26.464295] addr 0x1f: write:0x6d ,read:0x6d
<4>[   26.466390] addr 0x20: write:0x71 ,read:0x71
<4>[   26.467142] addr 0x21: write:0x05 ,read:0x05
<4>[   26.467876] addr 0x22: write:0x0f ,read:0x0f
<4>[   26.468622] addr 0x23: write:0xb1 ,read:0xb1
<4>[   26.469364] addr 0x24: write:0x3d ,read:0x3d
<4>[   26.470685] addr 0x25: write:0xce ,read:0xce
<4>[   26.472152] addr 0x26: write:0x00 ,read:0x00
<4>[   26.472904] addr 0x27: write:0x4f ,read:0x4f
<4>[   26.473669] addr 0x28: write:0xd1 ,read:0xd1
<4>[   26.474433] addr 0x29: write:0x2c ,read:0x2c
<4>[   26.476509] addr 0x2a: write:0x7f ,read:0x7f
<4>[   26.477253] addr 0x2b: write:0xb6 ,read:0xb6
<4>[   26.478022] addr 0x2c: write:0x80 ,read:0x80
<4>[   26.478906] addr 0x2d: write:0xae ,read:0xae
<4>[   26.479817] addr 0x2e: write:0x7e ,read:0x7e
<4>[   26.480559] addr 0x2f: write:0xfc ,read:0xfc
<4>[   26.481291] addr 0x30: write:0x7f ,read:0x7f
<4>[   26.482058] addr 0x31: write:0x52 ,read:0x52
<4>[   26.482807] addr 0x32: write:0x81 ,read:0x81
<4>[   26.483572] addr 0x33: write:0x4c ,read:0x4c
<4>[   26.485032] addr 0x00: write:0x00 ,read:0x00
<4>[   26.486295] addr 0x3f: write:0xf4 ,read:0xf4
<4>[   26.487502] addr 0x40: write:0x00 ,read:0x00
<4>[   26.488923] addr 0x00: write:0x01 ,read:0x01
<4>[   26.490310] addr 0x20: write:0x86 ,read:0x86
<4>[   26.491632] addr 0x20: write:0x86 ,read:0x86
<4>[   26.492843] addr 0x20: write:0x86 ,read:0x86
<4>[   26.494057] addr 0x2a: write:0x0c ,read:0x0c
<4>[   26.495235] addr 0x2a: write:0x0c ,read:0x0c
<4>[   26.496483] addr 0x2a: write:0x0c ,read:0x0d