Part Number: TPA3116D2
Other Parts Discussed in Thread: TPA3130D2, TPA3118D2, , TPA3251, TPA3221
I have few questions about this Class-D amplifier chip, which are not clear and can't be found in the datasheet.
First of all, what is the DC voltage offset on the input pins (4,5,10 & 11) .
Is that just 1/2 PVCC?
Although the datasheet also states that the maximum input voltage can only be 6.3V max.
Seconds question, what is the real difference between the TPA3116 and TPA3118 (and even the TPA3130) ?
According to the datasheet, the only difference between the 3116 and 3118 is the position of the thermal pad.
However, that would mean that if you would make the cooling adequate enough, the TPA3118 could also deliver 2x50W?
The datasheet also only mentions one Rds(on) value, so that would suggest that the TPA3130 is the same as the other two.
The only clear difference is in the thermal information. Although, ones again the TPA3118 has similar or even better results compared to the TPA3116.
What are the physical differences between the three?
Last thing, is there any information about oscillation frequency and performance?