This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Excuse me Will PCM2903 support the following OS?
Windows Server 2012 R2 64bit
Vmware ESXi 6.0 UI 64 bit
Ubuntu 15.1 or later 64 bit
Hi, Allan,
The PCM2903 should be able to operate with any operating system that supports USB Audio Class devices; the PCM2903 operates with the native OS USB-audio driver. Actually, please make sure the 'C' Version of the device is used as it has some fixes made to the original release device.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer