Part Number: DRV135
Other Parts Discussed in Thread: DRV134, INA137, OPA1678
Hi
I am developing a project on audio transmission where it is required to send audio signals over long distance (30m) long via wires using mobile phone audio output. the audio output is fed to a dc 15V 10w audio amplifier and then to the line driver DRV135. at the receiver end the incoming differential audio signal passes through the INA 137 which is then amplified by the amplifier and gives output to the speakers.
Please help is this the right approach, I am a bit new to the audio transmission. I have used many amplifiers before but not transmitted the signal to large distances.
Regards
Pranav Dosajh