Hello,
I'm reviewing a circuit with a TLV320AIC3204 that is connected to a Huawei modem. This circuit is working, but there must be something wrong because after some time (months working) the TLV320AIC3204 crashes and the worst thing is that it breaks I2C communication with other peripherals. I'm trying to detect what is the problem, but I don't get it.
There is only one thing that is happening and i think it's not normal. I connected a zenner diode into IOVDD because PCM levels in the modem must be 1.8V, but I've measured with a multimeter and I get around 3 volts into IOVDD. I will check PCM levels with an oscilloscope, but this is strange. On the other hand, I'm configuring the audio codec through I2C (3.3 level). I say so, because I'm working with different digital value levels, but there is only one IOVDD supply. So, is this one maybe the cause for the problem?
Thanks very much!