Hello,
Would you please answer the following questions ?
① Initial setting value of Control Register
What is the default value of the Control Register immediately after TAS 5411 - Q 1 is activated?
Is it the setting of 01111000 of the data sheet 19 page Table 8. Control Register (0x03)?
② Can I use the pullup voltage of FAULT Pin (14 pin) at 4.87 to 5.15 V?
③ MUTE Pin (8 Pin) is Active-high, but what is the threshold value for detecting high?
Best Regards, Orobianco