I have a question about pin assign of TAS6424-Q1 datasheet.
Target pins are STANDBY, MUTE, FAULT and WARN.
There are defference between Datasheet P.4 and datasheet P.54.
Which one is correct?
I believe P.4 is correct. Because it is same pin assign of user guide.
P.4 P.82
STANDBY 24pin 25pin
MUTE 25pin 24pin
FAULT 26pin 27pin
WARN 27pin 26pin
Datasheet P.4: 6 Pin Configuration and Functions
Datasheet P.54: Figure 82. 2-Channel PBTL Application Schematic
Best Regards,
Y.Hirata