This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2011D1: Asking for the TPA2011 datasheet's output power at 8ohm

Part Number: TPA2011D1

Hi Team,
My customer would like to check the following conditions output.
from 7.6 table, the output power is 1.46W which match with figure 11.
1.RL=8ohm,
2.THD+N=1%,
3, f=1kHz

However, the figure 10 output power is close to 2Watt which is different than the 7.6 table and figure 11.

Could you please provide your comment for why the figure 10's output power is close to 2Watt?

Thanks,
SHH