This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM5142: PurePath multiple sampling rate question

Part Number: PCM5142

As I understand, I need multiple binaries - one for each sampling frequency, as a sampling frequency change will require changes in the filters coefficients. So if my input is the range of 44.1 up to 192Khz, I need a variant of the binary to allow that.

So if I have a crossover at 200hz, I need a binary for 44.1, 48, 96...192 to cover all audio streams. And for crossover at 190, a similar series. I can create the configurations for the different crossovers, but I have not found a way to specify configurations with different sampling rates.  Below is an example of filter properties notice run-time properties is defaulted to 44.1. I do not see a way to change that or to cause different configurations to be built. Thank you for any assistance.