Hi,
I am trying to capture sound from TLV320AIC3105 MIC1L/LINE1L and use left-ADC, but I get none. Here are the register settings for capturing:
Page 0 /Register # |
Value |
2 |
0x00 |
3 |
0x20 |
7 |
0x0A |
8 |
0xC0 |
9 |
0x00 |
10 |
0x00 |
12 |
0x50 |
15 |
0x7F |
16 |
0x7F |
19 |
0x04 |
22 |
0x04 |
25 |
0xC6 |
|
|
37 |
0xC0 |
41 |
0x00 |
43 |
0x00 |
46 |
0x00 |
47 |
0x80 |
|
|
101 |
0x01 |
102 |
0x02 |
I also tried to add AGC, here is AGC settings:
Page 0/Register # |
Value |
26 |
0x80 |
27 |
0xFE |
28 |
0x3F |
|
|
34 |
0x12 |
|
|
I found, after capturing, ADC PGA is changed to muted, LINE1L is not connected to the Left-ADC PGA. I am not sure if it is normal or not.
For this test, TX clock is used for both TX and RX, codec is set as master.
Is anything I am missing and doing wrong?
Regards,
Bruce