Other Parts Discussed in Thread: RM57L843
Hello!
I need to convert the ".wav" file which is " Linear PCM" digital audio to analog. S can I convert it with a DAC or I have to use a PCM CODEC?
Also Suggest me a Part number.
thank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: RM57L843
Hello!
I need to convert the ".wav" file which is " Linear PCM" digital audio to analog. S can I convert it with a DAC or I have to use a PCM CODEC?
Also Suggest me a Part number.
thank
Hi, Zain,
Thanks for the feedback.The codec or DAC selection depends mostly on the end-requirements of your system in terms of power, number of outputs, performance, etc. Almost all of our devices can operate with 16-bit data so that is not an issue, but the available output formats that your processor can handle should match the codec/dac specs. If you don't need analog to digital conversion, a DAC should be a better option.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi Deigo!
Thanks for your support. I found my answer.
Regards
Zain Ul Abideen
Hardware Design Engineer.