Other Parts Discussed in Thread: TAS5766MDCAEVM, TAS5766M
Good day,
I am currently evaluating the TAS5766 using the TAS5766MRMTEVM connected to the PurePath Console Motherboard. Doing the "System Calibration" is entirely successful as can be seen below but when I click on "Tuning and Audio Processing" it runs through a number of things on the bottom left of the screen but after it does "Updating coefficients to device..." it seems to stop doing anything as shown in the second picture. It does not progress from this point even if left for extended periods of time. When I Monitoring the I2C lines between the motherboard and EVM with an oscilloscope I can see all the communication up until it stops where all communication seems to stop as well. I am not sure whether it is waiting for a response from the EVM. I have also noticed the PurePath Console hasn't frozen and I can still click close and it prompts me if I would like to save.
Using "End System Integration" I am able to dump to a header file (I can see I2C data being written and received when I do this).
I have tried the following to no avail:
- Tried reinstalling PurePath Console 3
- Tried PurePath Console 3 on two separate laptops (one Windows 10 the other Windows 7)
If anyone has any additional suggestions or fixes I would be very grateful.