This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5756M: 【TAS5756M】What are the modules in DSP after providing the reference signal?

Part Number: TAS5756M


Dear,

    As note,my register setting like below;(SDOUT is the DSP output (post-processing))

           //////// reg[0][7]
           { 0x07, 0x00 },
           //////// reg[0][8]
           { 0x08, 0x20 },
           //////// reg[0][85 ]
           { 0x55, 0x07 },
   

    1: In HYBIRDFLOW 1, what are the modules in DSP routing after the SDOUT reference signal?

    2:  In HYBIRDFLOW 4,  what are the modules in DSP routing after the SDOUT reference signal?