Hi Tis,
There are some questions about the analog input level of aic3268
Please help me check!
(1) There are a singled-end stereo line in(connector is phone jack) and a differential stereo line in(connector is XLR) in our product design. We wish that the line level of phone jack is consumer line level(about -10dBV, 0.316Vrms) and XLR is professional line level(about +4dBu, 1.23Vrms). Per aic3268 datasheet, the max input signal level of singled-end is 0.5Vrms and differential is 1Vrms(CM=0.9V).So it seems the consumer line level is OK but professional line level is over. If we want to support the professional line level in differential input, how could we do ?
(2) Could we choose the large input impedance such as 40Kohm to support the analog signal with higher level(>1Vrms)? With 40Kohm input impedance, the differential input level reduce 6dB before PGA mixed. So the differential signal level could up to 2Vrms. is it correct or wrong?
Thanks!
BR,
Steven