The device generate a FAULT signal, and stop operation when output voltage level approach the supplied voltage.
The supplied voltage is set to 50 Vdc and upon the output voltage reaching ~45 V, the device cuts off.
Reducing the supplied voltage to 45 Vdc, the cut-off occurs in 40 V, looks like around 5 Volts headroom ????
As output voltage approaching the supplied voltage, I expect to see some clipping on the output, but the device never get into clipping,
it just cuts-off, and recovers a second later. Keeping the the output voltage at the same level, will cause the device to tuns OFF and back
ON at a rate of about one sec.
I would appreciate any suggestion or hint for the possible reason for the described issue.
Best,
Ron