Other Parts Discussed in Thread: TAS5414C
Hi
I have a question of Load diag.
According to datasheet, it says load diag test takes approximately 229ms to run.
I will include discharge (75ms), ramp up (52ms), check (50ms) and ramp down (52ms).
However, datasheet says if a fault is present or large capacitor to GND is present on output, check phase will repeat up to 5 times.
So if a fault is present during load diag, check phase (50ms) repeat 5 times additionlly and takes additional 50 ms x 5 = 250 msec?
If yes, total diag time will be 75 + 52 + 50*6 + 52 = 479 msec as maximum. Is it correct?
BestRegards