About TLV320DAC3203 DAC function, please let me check about BiQuad x 3+DRC and DAC fs=16kHz solution below.
-----------------------------------------------------------
①I think that recommend way is choice below application note Page-23, PRB_R1~PRB_R18.
In thin case is match the PRB_P5, is it correct?
②If ① is correct, unnecessary BiQuad are No=2~23,and set to N1=N2=D1=D2=0, is it correct? (In the Mono condition)
③Is interpolation filter need to set "A"? (Because DAC_FS=16kHz condition)
④About DRC, HPF cutoff is default: 0.00166*DAC_FS, LPF cutoff is default: 0.00033*DAC_FS.
I think that in the case of HPF and LPF both using, it have no bandwidth.
This meaning DRC is not perform in default and should change set point of conforming with condition, is it correct?
-----------------------------------------------------------
Best regards,
Satoshi