Part Number: PCM2904
Dear fellow developers,
I am currently designing a system which includes the PCM2904. In order to optimize the power managemant subcircuit (and to stay USB compliant) I would need the enumeration status of the device. I am particulary interested in the assigned maximum current. The PCM2904 does have a 500mA descriptor, but if the system cannot meet the requirements - how will I find out? Or more precisely:
Is there any way to retrieve the enumeration status from the PCM2904?
Kind regards