Hi, everyone.
I have read this thread:

It did can output signal. But it is not the way provided by data sheet.
I measure the phase it have delay about 4.5 ms. (this should not be that long delay in hardware)
The data sheet say we should use MISO or SCLK as output PDMCLK. Not BCLK.
So what is the right way using MISO(as an output PDMCLK) to receive digital microphone signal then output the signal to HPL and HPR?
I would like output a 2.048MHz MISO (Assume I provide a crystal clock with 4Mhz into MCLK) and have the digital microphone signal at HPL (R) pin?