Part Number: TLV320DAC3203
Hi~
I have read this thread:
and what I concern is that BCLK as PDMCLK input is not provided by datasheet.
The datasheet say PDMCLK should be set at MISO and SCLK pin.
My concern is that the receiving data might not be right. When I measure the delay of the signal, it is very high, about 4.5 ms.
Is there a way by using MISO as PDMCLK and DIN as input data then output signal to HAL (R)?
The sample code in data sheet is useless because I cannot check if my Dmic receive the correct signal.
Thx