TAS5421-Q1:
What happens, if I add a small DC Voltage like 30mV between OUTP and OUTN? Lets assume it is done with connecting a resistor between PVDD and OUTP and another one between GND and OUTN so that a drop of 30mV is at the Speaker and thus at OUTP-OUTN and centered around PVVD/2.
Let's assume, that this is established after the device is in unmuted play mode and no Errors have occured.
Does the TAS5421 indicate a fault? Like the "DC Detect"?
Another question would be: What exactly is the DC detection threshold (see chapter 7.3.6 in SLOS814C)?