This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424-Q1: we need your help, source code ( program ) for transfer with Atmel Studio to Attiny24

Part Number: TAS6424-Q1
Other Parts Discussed in Thread: TAS6424

hi Guys,

we need your help, our programmer is ill ... !

we must program a Attiny24 and for that we need the source code for Atmel Studio.

who can write us the source code, we also pay for the trouble.

we have the PPC3 and the TAS6424-Q1 EVM.

please save as PPC3 file and the source code ( program ) for transfer with Atmel Studio Programmer to the ATtiny24

if you use the MSP430 syntax, i think we can try to replace it with I2C comands

source code ( program ) Setup:

0. Channel Fullrange ( Midrange 4 Ohm ) =   Volumen 0 dB ( Volume +/- adjustable / variable )
1. Channel Fullrange ( Tweeter 4 Ohm )   =   Volumen 0 dB ( Volume +/- adjustable / variable )
2. Channel Fullrange ( Bass Coil 2 Ohm ) =   Volumen 0 dB ( Volume +/- adjustable / variable )
3. Channel Fullrange ( Bass Coil 2 Ohm ) =   Volumen 0 dB ( Volume +/- adjustable / variable )

1. Bypass diagnostis = switch off
2. Temperatur = setting Temperature warning to 140 degree (max)
3. Clip and overtemperature warning ( switchable on or off ) Pin 27 / Warn
4. Reports a fault ( switchable on or off ) Pin 26 / Fault
5. Mutes the device outputs ( switchable on or off ) Pin 25 / Mute
6. Enables low power standby state ( switchable on or off ) Pin 24 / standby
7. Voltage automotive 14,4 Volt = Set Gain to Level 2 (15V)

For your help we are very thankful....

Have a nice Weekend ....

with kind regards

ATE Norman