Part Number: TAS5751M
I am building a board with the TAS5751M. I cannot get any audio out. The I2S signal "looks" good and I do not get any errors reading registers 0x00 and 0x02
When I inspect the output before the LC filter, I noticed a difference from the EVM. I reviewed the difference between AD and BD modes (http://www.ti.com/lit/an/sloa119b/sloa119b.pdf
When I change the settings between AD and BD (registers 0x11~0x14) I do not see any difference in the switching output So the two issues:
1) I cannot get any audio out from the amplifier
2) changing the modulation mode between AD and BD has not effect on output switching
So not sure if the problem is in the I2S signal, the modulation scheme etc.
Screenshot of I2S signal with no audio input (LRCLK and SDIN)
Screenshot of the test board output switching (AD and BD is same)
Screenshot of EVM switching in BD mode
Schematic
I2C traffic of simple initialization/bootup (in BD mode)