Part Number: LM4864
Other Parts Discussed in Thread: TPA0211, TPA0213, TPA6203A1, TPA6211A1
Dear Sirs,
We have developed electronic equipment for the agricultural sector. Now we are finalizing the development of a HMI device, similar to a tablet. But, more robust and for agricultural applications.
As processor, we are using a Toradex SOM, line Colibri iMX6. I need in this project an output for a Speaker. I do not need high sound quality. I just need a volume that is enough to be heard inside operating cabins.
I need a speaker to play only alerts / warnings. I need to developed one hardware using the module's headphone output (or another audio output). After that, I needed one amplifier to play a Speaker.
Is it possible to indicate some PN for this application?
For testing, I developed a PCI with the LM4864 amplifier on the Headphone output of the module. For Speaker, I used one 8Ohms / 0.5W CUI Speaker.
However, the sound output on the Speaker is very, very low even at maximum volume.
To help, I've attached the schematic I used for the LM4864.
Actually I'm not sure if I did something wrong with the LM4864, or if the output power to my application should be higher - and how much?
Kindly,
Daniel MartinsSchematic LM4864.pdf