I am trying to update the firmware for my TLV320ADC3101EVM-K kit in order to work with PurePath Studio. I am running Windows XP SP3. Following the instructions, I installed the DFU driver and my OS recognizes the device perfectly fine. But When I launch DFUTEST.exe, click on "Program EVM" and select DFUEE, I get a prompt message saying, "Device was successfully reset. Please wait about 2 seconds for device to re-enumerate." Then I click OK and get the Error prompt saying "Detach call failed". What am I doing wrong here?
I am following the procedure as follows mentioned in another forum and the answer was provided by Dominik Hartl11:
* flip the SW2-A2 switch on the USB modevm to the right (HI).
* connect the EVM to the PC and follow the instructions to install the TI DFU driver (in the attached zip)
* once the driver has installed, flip SW2-A2 to the left (LO).
* launch DFUTest.exe
* click Program EVM, choose file DFUEE.bin (in the attached zip) and follow the on-screen instructions
* choose USB-miniEVM0204_441kHz.bin (or a .bin file with the desired sampling rate) and follow the on-screen instructions
* disconnect the EVM and re-connect the EVM.
Thank you,
Kishan Patel