This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254EVM-U: TLV320AIC3254EVM-K

Part Number: TLV320AIC3254EVM-U
Other Parts Discussed in Thread: TLV320AIC3254EVM-K, TLV320AIC3254

Hi All,

 Now I using  the communication  between Master and TLV320AIC3254EVM-K Via I2S . Moreover, I using  I2C  interface is to config I2S mode. You can see schematics below :

   Please help me confirm this schematics. I will appreciate for this support.

  • Hi, Toan,

    The schematic of the TLV320AIC3254 seems correct. I would recommend to put a 1µF cap connected from the input pins to GND if they are being unused. This is the suggested termination for the unused input pins.

    Regards,

    -Diego Meléndez López
    Audio Applications Engineer