//PLL 48KHz//
I2C1_Write(3,0x81); //PLL_EN=1(D7),PLL_Q=0(D6-D3),PLL_P=1(D2-D0)
I2C1_Write(8,0xd0); //BCLK&WCLK output
I2C1_Write(4,0x20); //PLL_J=8(D7-D2)
I2C1_Write(5,0x1e); //PLL_D_MSB(D7-D0) D=1920-----48k
I2C1_Write(6,0x00); //PLL_D_LSB(D7-D2)
I2C1_Write(11,0x01); //PLL_R=1(D2-D0)
delay_ms(100);
I2C1_Write(2,0x00); //Fs = Fs(ref)
I2C1_Write(12,0x44); //Left-ADC high-pass filter frequency = 0.0045 Fs,Left-DAC de-emphasis filter enabled
I2C1_Write(17,0x0f); //route Mic2L to the Left ADC, 0dB,
I2C1_Write(19,0x7c); //Left-ADC channel is powered up
I2C1_Write(15,0x28); //unmute Left PGA, set gain to 20 dB
I2C1_Write(7,0x0A); //Left-DAC data path plays left-channel input data
I2C1_Write(37,0x80); //Left DAC is powered up, HPLCOM configured as differential of HPLOUT
I2C1_Write(43,0x00); //The left-DAC channel is not muted,0db
I2C1_Write(47,0x80); //DAC_L1 is routed to HPLOUT,0db
I2C1_Write(14,0x80); //Programs high-power outputs for ac-coupled driver configuration
I2C1_Write(51,0x0f); //HPLOUT is not muted,HPLOUT is fully powered up,0db
Thanks ahead!