This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5756M: Power dissipation on +3V3 supply for DVDD, AVDD and CPVDD together

Part Number: TAS5756M

Hi,

I would like to know how much current a TAS5756M would consume from the +3V3 supply used for DVDD, AVDD and CPVDD.

There is a table "power dissipation" on page 23 of the datasheet which contains a column for IDVDD, but not IAVDD nor ICPVDD.

At some places however the datasheet refers to all +3V3 supply pins (so DVDD + AVDD + CPVDD) by simply calling them all "DVDD"; like for example in the "power supply recommendations"-section on page 82.
Is this also the case in the table on page 23? So, IDVDD is actually refering IDVDD + IAVDD + ICPVDD?

If yes: it is safe to say one TAS5756M will never sink more than 35mA from the +3V3 supply, used for DVDD, AVDD and CPVDD.
If no: one TAS5756M will never sink more than 35mA for DVDD alone, but how much current will AVDD and CPVDD sink then?

Thanks in advance!
Kind regards.
Julien