This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2900C: PCM2900C oscillator disables and system fails connecting USB

Part Number: PCM2900C


Hello,

i am trying tu use a PCM2900C Audio Codec, we want to use it in a record player.

I created a test PCB according to datasheet  Page 26/Figure 38.

I think i did a clean layout, short connections..., i checked all voltages  of on Chip VR's, all seems ok.

Data lines 22R and 1,5k resistor versus D+ on  data lines are present of course.

I always get message when connecting to USB under Windows "USB-device not recognized". 

On XTO i can observe a 12MHz  signal after connecting until this message pops up, then XTO goes high-

I tried to add additional decoupling cap's of 10nF in parallel to proposed 1uF/10uF caps without success.

Then i realized that coming near data lines with my finger 12 Mhz suddenly starts again, i tried to different test PCB's.

I experimented a little and found out that clock becomes stable, if i connect D* and D-Input with a 10K resistor, Data lines not connected to USB.

So one question:

Is XTAL oscillator supposed to run permanently , when powered? or is it disabled when USB fails connecting?

Datasheet does not show anyting about a internal disable/option in PCM2900C's functional diagram.

perhaps somone can help me

best regards

Wolfgang