We have a board using the TLV320AIC3206 with AC-coupled, differential, analog input signals. -- schematic below. However, we are not able to measure the expected 0.9V common-mode voltage on the analog input pins (and the analog inputs are just noise when digitized or routed through to the headphone outputs). The voltage on all 4 input pins measures as 0V -- even with all the protection diodes and the AC coupling capacitors removed (so completely open-circuit). The REF pin of the CODEC is 0.9V as expected, and the 1.8V and 3.3V power rails are present and look clean. Are there any hardware issues apaprent with this design? Are there software configuration settings that we should be checking? Thanks,
However,