This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIX4192: Vih/Vil spec of RX

Part Number: DIX4192


Hi,

I would like you to confirm about threshold of RX signals.

According to datasheet.

1. Each RX is biased by 0.5 * Vcc (In fact generated by dividing resistance (24k ohm))

2. "differential input sensitivity" is defined "max = 200mV"

From above information, I guess that Vih for following each case are defined as shown below. Is my understanding correct ?

In case of Single End (RX- is connected GND).

* RX+ : Vih(min) = (0.5 * Vcc) + 0.2V (Ex. If Vcc = 3.3V, Vih(min) = 1.85V)

In case of Differential.

* RX+ : Vih(min) = (0.5 * Vcc) + 0.1V (Ex. If Vcc = 3.3V, Vih(min) = 1.75V)

* RX- : Vih(min) = (0.5 * Vcc) + 0.1V (Ex. If Vcc = 3.3V, Vih(min) = 1.55V)

I woluld like you to confirm whether we can also understand "differential input sensitivity" mean threshold of Vih/Vil or not.

Best Regards,