Part Number: PCM2912A
Dear Sirs,
My customer use PCM2912A for Mic input to their system via USB port.
There is a question that while there is mic signal input, they can hear it from speaker at same time.
Is it possible to turn it off?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM2912A
Dear Sirs,
My customer use PCM2912A for Mic input to their system via USB port.
There is a question that while there is mic signal input, they can hear it from speaker at same time.
Is it possible to turn it off?
Thanks.
Hi, Peter,
This part features a Mic mute option by sending a logic HIGH signal to MMUTE pin. However, this option mutes the input mic, not the speaker output playing the audio signal from the mic.
Could you please clarify if the speaker that plays the mic content is in the host system?, it is possible that the Listen to this device option is enabled by the computer in the PCM2912A from the recording devices window.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi Diego,
Below are some testing by customer.
1. while mute enable, the Mic signal will stop to output to USB, however, the internal route to spk still have output
2. under WINXP, if not run record program, the Mic sound will not be gear in PC output.(assign output with another sound card), but there is output from PCM2912A
3. Under WIN7, same situation with WINXP, assign output with another sound card, it needs to check "listen to this device" to make it output.
Meanwhile, PCM2912A always has output even check or uncheck this setting
4. it seems PCM2912A still always output its Mic signal.
Please help to check it.
Thanks.
Hi, Peter,
Thanks for the additional information. The device should not playback the content from the mic recording, it is not a normal behavior. What customer is requiring is exactly the normal behavior of the device. I have tried my EVM and was able to verify this behavior. The only way to send the mic content to the headphone output is by checking the Listen to this device option.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi Diego,
Let me clarify the request from customer.
What customer need is, while Mic input from PCM2912A, they do not want to hear the Mic input from PCM2912A headphone output.
Actually, it seems PCM2912A will loopback the EVM mic input to EVM headphone output at any time unless you disable PCM2912A.
Hi Peter,
This is what I am mentioning in my previous response, the PCM2912A should not playback the mic input through the HP outputs unless the host device configures the device to do that. A possibility is that the device has been configured with the side tone option enabled, which will send mic content from the recording signal to the headphone output. Can you please verify in the recording devices window if the PCM2912A [USB AUDIO CODEC] has the microphone signal muted under the Levels tab?.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi Diego,
Thanks for your reply!
Below pic is my test device and configuration.
As you can see, the "listen to this device" did not check, but I can hear the mic voice from PCM2912A headphone, not NB headphone.
That is what customer did not want to hear.
You can take it try with my way.
Is there any way to turn off the mic loop back to PCM2912A headphone output?
Thanks.
Hi, Peter,
As I mentioned in my previous reply, it is possible that the device has the "Side Tone" volume enabled. This feature was used in the past as a mic feedback for the user to monitor himself, you can use a phone call for example. This device has the option to change the level/Mute the side tone under the Levels tab of the properties window:
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi Diego,
After test, mute mic volume in level tab is not work for me!
I found it works if I mute mic in speaker tab.
However, customer system is not Win OS! he connected PCM2912A board via OTG cable into their system.
Is there any way to change any setting in such situation?
Thanks.
Hi, Peter,
I noticed my picture was not uploaded correctly, please refer to below:
Is this the same method you tried in your end?.
Windows just provides a visual way to mute the Side tone Function of the PCM2912A, it is up to Customer OS to disable this feature on the device. I am not familiar with the internal process to disable this feature on terms of USB protocol.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer