This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5756M: TAS5756 GVDD Two-Step Ramp Up Sequence

Part Number: TAS5756M

Hi Sirs,

Would you pls check if my GVDD ramp up sequence in line with our device specification that the GVDD ramps up to 5.3V with PVDD and ramps up to 7V with I2S DIN ON? If yes, what is the GVDD's first step's voltage specification? My measurement was 5.3V while we need a range for customer's system level verification.



GVDD ramps up to 5.3V with PVDD



GVDD ramps up to 7V with DIN ON





Thanks a lot

Wayne Chen
01/16/2018