Other Parts Discussed in Thread: TINA-TI, TPA3255
I see on the first page of the TPA3244 datasheet that the device supports "Signal Bandwidth up to 100 kHz...".
I have an application that requires passing more sinusoidal-type signals close to that 100kHz frequency. However, I don't see any characterization of performance at these high frequencies in the datasheet. Is there any such data, to see if there is any rolloff at high frequency?
When using the LC Filter Calculator excel tool, I can say I want a cutoff freq. of 200kHz, which allows for acceptable filter behavior at 100kHz, but the inductance required is ~2.25uH, which appears to be below the recommended minimum inductance of 5uH, per TPA3244 datasheet. Is there some way to safely operate TPA32xx with lower than recommended inductance values?
My load does not necessarily have a flat frequency response, thus the "peakiness" that I see at various load impedances with the chosen LC filter values are of concern. Would Post-Filter Feedback help to mitigate this issue, and if so, can it be simulated in TINA-TI, along with a model of my actual load?
Since I would like to operate at a much higher than typical audio frequency, the LC filter cutoff frequency necessarily has to be higher than typical with TPA32xx applications. Would it be beneficial to operate TPA32xx in AM2 mode (highest switching frequency), in order to get more attenuation of the switching frequency components on the output?
Thanks!