This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

find a part which can replace REALTEK's ALC5633Q

Other Parts Discussed in Thread: TLV320AIC3212, TLV320AIC3110

Hi,

One of my major customer would like to replace ALC5633Q to proper TI part if possible.

Below is ALC5633Q datasheet. (I2C + I2S Stereo Audio Codec + Mono Class-AB/D Amp)

ALC5633Q.pdf

They want "SPEAKER Amp, Mono 1w+, I2S support, MIC1, Audio Codec".

Please share the infomation about suitable TI device.

thanks,

TS

  • Hi, TS,

    There are a couple devices that could be considered to replace the ALC codec. It would be good if you can provide more information about your customer needs, like Stereo Vs mono ADC/DAC, target SNR, desired processing, etc.

    A device that could meet all the specs from the ALC part is the TLV320AIC3212, this part has an integrated Stereo Class-D Amplifier and meets the rest of the requirements mentioned. However, this is a more integrated part which may be too much for customer's application.

    Another option would be the TLV320AIC3110. This codec has a Stereo Class-D amplifier and Mono ADC for a mic input. If single ADC is acceptable, this might be a better option.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer