Other Parts Discussed in Thread: INA217, PGA2310
I'm working on a design for an audio mixer for a small recording studio and have succesfully tested the schematic for the INA217 published as Figure 4 on page 7 of the TI data sheet: http://focus.ti.com/lit/ds/symlink/ina217.pdf
I'm very pleased with the response of the published circuit, but I'd like to do a few modifications:
1. I'd like to provide an alternative input for an unbalanced, high impedence source (i.e. electric guitar, etc.) so that the circuit could be run on either source.
2. I'd like to add a pad or "trim" control in front of the IC to prevent a source signal that is too "hot" from overdriving the IC.
3. I also wonder if the gain control potentiometer, R7, could be eliminated, leaving R6 at a fixed value of 8 ohms, to run the IC at maximum gain, then adjusting the volume with a variable resistor in series with the output of the IC. This would allow for other subsequent stages at the output side including EQ, AUX I/O effects, etc. before hitting the main fader.
Comments please!