Part Number: TPA3140D2
Hi,
I am designing a PCB using TPA3140D2. I was referring to datasheet as well as EVM user guide for reference Layout designing. I have little confusion on following
1. AVCC pin connection with PVCC: Datasheet suggest 10E resistor, EVM shows direct connection, which should I implement? In case of resistor, what should be the value of resistor/what is current requirement for AVCC pin?
2. Capacitor at AVCC pin (1uf to 10uF) is recommended in datasheet but not implemented in Eval board. Can this be dropped?
3. Do we need a resistor between 1SPW and AVCC?
4. Do we need RC circuit at the Audio output pins? (not there in datasheet but used on EVM). Also, is it ok to have provision for these on board and not mount them? will the open stub cause any issue?
5. Recommended layout shows straight traces for audio out but traces on EVM are not running that straight, is it OK if I follow trace pattern observed in EVM. I am planning to use 0603 components and thus will not be able to run traces straight. Let me know if I can bend them a little (as in EVM) or should change components to 0402.
6. Also, I am planning to connect capacitors at bottom side for Power trace and Audio out traces, connecting them to top traces using Vias, is this OK? Though this is not shown in either of the document, I wanted to know this in order to keep capacitors closer to pins.