I have a customer who is seeing failures when he runs tests that short the outputs to either GND or to other output. The data sheet indicates that the TPA2011 should not encounter these issues and should be able to withstand a short to GND or to the other output. The only difference I have noted in looking at this issue with the customer is that the failures seem to be when the customer has an additional LC filter attached to the output. When he uses a ferrite beads and a 1nf cap vs. an LC type filter the failures do not occur. Are the failures related to the additional circuitry? Is the device designed to be able to withstand a short and restart without damaging the part?
Thanks for your help with this!
Richard Elmquist