Hi,
Is there also a Tina model or a Tina reference design of the TPA6120A2?
The offset voltage is a bit high for my liking and I usually implement then a servo amplifier to zero out the output DC voltage.
I have built such a topology and it works fine
I use the TPA6120A2 as output driver for a low noise, low distortion tone generator.
I want to add a constant output impedance voltage divider on the output to allow for mV level output signals and maintain SNR, hence the divider.
The combination of the output divider and servo amp might cause unforeseen effects on the phase margin which is easier to check using a simulation tool.
Thanks for the feedback.