Part Number: SRC4193
Dear TI E2E members,
i would like to use this IC in a prototype DAC project, but i am having a hard time understanding the automatic sample rate detection. Let's say i have a 24bit I2S signal with a 32bit frame, coming from a USB to I2S converter. The Fs can be 44.1, 48, 88.2, 96, 176.4, and 192kHz. What i need is a constant 192kHz 20bit left justified signal, no matter what the input frequency is. This is where this IC would come in, but the automatic sample rate detection is confusing me. If i select the 20bit left justified output, how can i set the 192kHz? Is it defined by the input reference clock, or the BCKO in slave mode? If so, do i have to calculate the clock speed like this: 192000 * 2 * 32, or like this: 192000 * 2 * 20?