Hi team,
I posted a thread in below link before.

To the questions,
1. I2C address 0x18 is correct. Customer use Linux, and I2C driver can convert 0x18 to 0x30, the registers are being correctly configured by reading them back.
2. Change is PLL settings, the same prolbem.
CODEC_CLKIN = MCLK
PLL = OFF
NDAC = 1
MDAC = 2
DOSR = 128
3. The X symbol on on pins 3, 13, 14 19, 22, 23, 26 and 31 is for electrical rules check, should be no problem.
4. There is NO PWM signal coming out of pins 19, 22, 23 and 26? And also there is NO offset voltage coming out of pins 27 and 30, that means HP and Class-D are not powered up. But the power is already applied to AVDD/DVDD/IOVD/SPKVDD.
Besides Power up sequence, any other possible reasons for this issue?