Part Number: PUREPATH-CMBEVM
Other Parts Discussed in Thread: TAS5766MRMTEVM, TAS5766M
Using the PUREPATH CMBEVM Rev. G with a TAS5766MRMTEVM amplifier module.
Running the test boards with PurePath Console 3, at 48kHz sample rate, the MCLK frequency is 12.288 Mhz.
I want to use an external PSIA source that provides a 24.576Mhz MCLK. I'm pretty sure I can find the registers to change the SCLK/BCLK ratio in the TAS5766. but any time-saving hints would be welcome-- should I use the three-wire PLL mode instead? :)
My main question is, do I need to change the MCLK rate or other registers for any other components on the CMBEVM? I think the answer is no but I just wanted to check in first. Thanks!