Other Parts Discussed in Thread: SRC4392
Hello,
I would like to use the PCM5242 as follows:
- I2S slave mode, 3 wire interface without SCK,
- SCK via GPIO pin to DAC CLK Source Mux,
- SCK is powered by external oscillator with 45.1584 or 49.152 MHz,
The internal PLL is supposed to feed the DSP (I assume that jitter will not work here). A microcontroller selects the sampling frequency matching oscillator as DAC clock.
My questions:
- Does the DAC clock have to be synchon with the sampling rate (LRCK)?
- Does the DAC clock have to have a correct phase reference to other (external) signals?
- Or are deviations up to +/- 4 SCK allowed ("If the relationship between LRCK and system clock changes more than ± 5 SCK, internal operation is initialized within a sample period and analog outputs are forced to the bipolar zero level")?
- Is my assumption correct that the internal settings for the external DAC clock are made automatically ("The sampling frequency detector sets the clock for the digital filter, Delta Sigma Modulator (DSM) and the Negative Charge Pump (NCP) automatically.")?
- Are there already proven register settings for my project?
Thanks for your support!
Greetings from Berlin, Hans-Jürgen